:EUSage:STARt
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:EUSage:STARt <date-time>
Where <date-time> is a string in the format mm/dd/yyyy hh:mm:ss.
Query Syntax
:EUSage:STARt?
Query Response
mm/dd/yyyy hh:mm:ss
Description
Sets the start time of the diagram's view port. The recorded data is not clipped. The format of the time argument is in the same format as is shown on the diagram for Start:
mm/dd/yyyy hh:mm:ss
Example
hwdiagram.write(':EUSage:STARt 04/23/2023 08:17:05')