:SYSTem:LKEY:SOFTware:SUPPort:EXPiration:DATE?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Query Syntax
:SYSTem:LKEY:SOFTware:SUPPort:EXPiration:DATE? "<model number>"
Where <model number> is the feature/model number string that identifies a Manufacturing , Research and Development , or Signal Integrity package license.
Query Response
<year,month,day>
Description
For the specified license package model number, returns software support expiration date in the form "year,month,day". For example, "2018,7,1". This is the date that the current licenses expires. This string is located inside the package license file and is listed in the following table.
| Parameter | Example Returned Feature/Model Number String |
Description |
|---|---|---|
| L-MFG | N1010200A | Manufacturing Package |
| L-RND | N1010100A | Research and Development Package |
| L-SNT | N1010300A | Signal Integrity Package |
Requires FlexOTO revision A.07.00 and above.
Example Query
:SYSTem:LKEY:SOFTware:SUPPort:EXPiration:DATE? "N1010200A"