:SYSTem:SOFTware:LICenses:BORRow?
Query Syntax
:SYSTem:SOFTware:LICenses:BORRow? <package license>, <number of days>
Where <package license> specifies the package license using the string listed in the following Software License Package Arguments table.
Where <number of days> is an integer that specifies how many days you wish to borrow the license. The valid range of days is 1 to 90.
Query Response
Boolean, 1 or 0
Description
Use this query to borrow a software license package from Keysight's Pathwave License Manager. You must specify both the package license and the number of days that you wish to use (borrow) the license. Be sure to separate the two arguments with a comma as shown in the example below. The query returns a '1' if the license was successfully borrowed and a '0' if the borrow failed. Always send the :SYST:SOFT:LIC:REFResh command before sending the :SYST:SOFT:LIC:BORRow query.
| Query Argument | Returned Description Name | Description |
|---|---|---|
| L-MFG | N1010200A | Manufacturing Package |
| L-RND | N1010100A | Research and Development Package |
| L-SNT | N1010300A | Signal Integrity Package |
Requires FlexOTO revision A.07.00 and above.
Example Command Sequence
The success variable will contain either a 1 for success or a 0 for failure.
FlexDCA.write(':SYSTem:SOFTware:LICenses:REFResh')
success = FlexDCA.write(':SYSTem:SOFTware:LICenses:BORRow? "L-RND", 5')
FlexDCA.write(':SYSTem:SOFTware:LICenses:REFResh')
success = FlexDCA.write(':SYSTem:SOFTware:LICenses:INSTalled? "L-RND"')