:SYSTem:SOFTware:LICenses:RETurn?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Query Syntax
:SYSTem:SOFTware:LICenses:RETurn? <package license>
Where <package license> specifies the package license using the string listed in the following Software License Package Arguments table.
Description
Use this query to return a software license package to Keysight's Pathwave License Manager. You must specify the package license. The query returns a '1' if the return was successful and a '0' if the return failed.
| Query Argument | Returned Description Name | Description |
|---|---|---|
| L-MFG | N1010200A | Manufacturing Package |
| L-RND | N1010100A | Research and Development Package |
| L-SNT | N1010300A | Signal Integrity Package |
Requires FlexOTO revision A.07.00 and above.
Example
:SYSTem:SOFTware:LICenses:RETurn? "L-SNT"