Polatis 6000 Switch Ports

Example Polatis Switch IDs

Because Polatis offers many configurations of installed switch modules, your switch may not match this picture. The following picture shows how the Polatis switch ports are named. The ID string for a port is simply an integer.

Available Port Connections
Front Panel
Switch Ports
Front Panel Label Out
(Ports 25 through 48)
In
(Ports 1 through 24)
Port Function in FlexOTO Inputs From Outputs To
DCA-M Modules ●
Fixtures ●
Demultiplexers ● ●
Impairments ● ●
User Instruments ●
Color definitions in table:
Switch ports that FlexOTO considers to be switch inputs.
Switch ports that FlexOTO considers to be switch ouputs.