:CRECovery:CLBandwidth
Command Syntax
:CRECovery:CLBandwidth <bandwidth>
<bandwidth> is a double.
Query Syntax
:CRECovery:CLBandwidth?
Description
Sets the loop bandwidth of the JTF Receiver module's clock recovery PLL in Hertz. Because jitter is measured relative to the clock, jitter that is present on both the data and the recovered clock can not be detected by the DCA-X. Jitter that is within the clock recovery module's loop bandwidth appears on the recovered clock. Jitter that is outside of the loop bandwidth does not appear on the recovered clock and can be detected on the data. Selecting the loop bandwidth allows you to eliminate jitter on the recovered clock. The loop bandwidth can be any bandwidth within 30 kHz to 20 MHz specified to 3 significant digits. The default setting is 60 kHz.
Command Compatibility
- 86108A/B
- 83496A/B Option 300
How do you identify the module's slot number location?
- In FlexDCA, the slot number is added to the subsystem name. For example,
:CRECovery2:CRATe. - In FlexPLL, the slot number is specified using the
:RDCA:CRECovery:SLOTcommand. The slot number is not used in the command. For example,:CRECovery:CRATe. From the GUI, enter the slot number in the DCA CDR Location field of the Receiver Setup dialog.
For FlexPLL application, requires revision A.06.70 and above.