:CRECovery Subsystem
Flex Apps:
FlexDCA
FlexRT
FlexPLL
For the FlexPLL application, the Clock Recovery subsystem commands control JTF Receiver module's clock recovery (N1060A Precision Waveform Analyzer module or an N107x-series DCA-M module). This includes setting data rates, as well as querying lock status and "signal present" conditions.
- Send the
:CRECovery:CRATecommand to specify the data rate (unbanded tuning). - Send the
:CRECovery:CLBandwidthcommand to specify a loop bandwidth. - Send the
:CRECovery:LOCKed?query to determine if the module is locked on the signal. - Sent the
:CRECovery:LSELectcommand to select the Type-2 PLL loop transition frequency (peaking). - Send the
:CRECovery:PRESetscommand to load a previously saved or factory provided clock recovery settings. - Send the
:CRECovery:RELockcommand to establish lock and to reestablish lock whenever a setup parameter changes (for example input port or trigger on data), the data rate changes, or the signal parameters change (for example, edge density). - Send the
:CRECovery:SOURcecommand to select between multiple module channels.
How do you identify the module's slot number location?
- In FlexDCA, the slot number is added to the subsystem name. For example,
:CRECovery2:CRATe. - In FlexPLL, the slot number is specified using the
:RDCA:CRECovery:SLOTcommand. The slot number is not used in the command. For example,:CRECovery:CRATe. From the GUI, enter the slot number in the DCA CDR Location field of the Receiver Setup dialog.