:CRECovery:SOURce
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:CRECovery:SOURce {ELECtrical | EINVerted | DIFFerential | OPTical}
Query Syntax
:CRECovery:SOURce?
Description
Selects the module's data input connector for clock recovery.
DIFFerential
Both front-panel electrical connectors with these labels:
- N1060A module: CHA/CDR+ and CHB/CDR– connectors
- N1076A/B, N1077A, and N1078A: Data + and Data – connectors
ELECtrical
Front-panel electrical connector with this label:
- N1060A module: CHA/CDR+ connector
- N1076A/B, N1076A, and N1078A: Data + connector
EINVerted
Front-panel inverted electrical connector with this label:
- N1060A module: CHB/CDR– connector
- N1076A/B, N1077A, and N1078A: Data – connector
OPTical
Front-panel optical connector. On N1077/8A modules, this is the DATA IN connector.
Command Compatibility
- N1060A
- N107X series
How do you identify the module's slot number location?
In FlexDCA, the slot number is added to the subsystem name. For example, :CRECovery2:CRATe. In FlexPLL, the slot number is specified using the :RDCA:CRECovery:SLOT command. The slot number is not used in the command. For example, :CRECovery:CRATe. From the GUI, enter the slot number in the DCA CDR Location field of the Receiver Setup dialog.