:CRECovery:LOCKed?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:CRECovery:LOCKed?
Description
Returns the locked status of the JTF Receiver clock recovery module.
The returned values are:
- 1
- Clock recovery is locked.
- 0
- Clock recovery is not locked.
Command Compatibility
- N107x-Series DCA-M
- N1092A/B DCA-M Option CDR
- 83496A/B
How do you identify the module's slot number location?
- In FlexDCA, the slot number is added to the subsystem name. For example,
:CRECovery2:CRATe. - In FlexPLL, the slot number is specified using the
:RDCA:CRECovery:SLOTcommand. The slot number is not used in the command. For example,:CRECovery:CRATe. From the GUI, enter the slot number in the DCA CDR Location field of the Receiver Setup dialog.
For FlexPLL application, requires revision A.06.70 and above.