:CRECovery:LSELect:AUTomatic
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:CRECovery:LSELect:AUTomatic {ON | OFF | 1 | 0}
Query Syntax
:CRECovery:LSELect:AUTomatic?
Query Response
{1 | 0}
Description
Turns on or off automatic selection of the Type-2 loop transition frequency (peaking) JTF Receiver module. When turned off, use the :CRECovery:LSELect command to manually select the frequency.
How do you identify the module's slot number location?
- In FlexDCA, the slot number is added to the subsystem name. For example,
:CRECovery2:CRATe. - In FlexPLL, the slot number is specified using the
:RDCA:CRECovery:SLOTcommand. The slot number is not used in the command. For example,:CRECovery:CRATe. From the GUI, enter the slot number in the DCA CDR Location field of the Receiver Setup dialog.
For FlexPLL application, requires revision A.06.70 and above.