| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property AdjustmentsEnabled As Boolean | |
| C# | |
|---|---|
public abstract bool AdjustmentsEnabled {get; set;} | |
When false, the adjustment properties (IQGain, QuadratureAngle, IQPhase, IQSkew, IQDelay, IOffset, QOffset) have no effect on the output signal.
When implemented by a Source, the return value is true if any of the source's channels with I/Q output have adjustments enabled.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)