For a list of all members of this type, see MeasurementExtension members.
Name | Description | Minimum SW Version | |
---|---|---|---|
![]() | CancelPulseDescriptorWordFileExport | Cancels an in-progress pulse descriptor word export operation. | 21.00 |
![]() ![]() | CastToExtensionType | This method casts the supplied object to the MeasurementExtension type. Some tools are unable to use the generic methods provided on Agilent.SA.Vsa.Measurement class so this is provided as an alternative. | — |
![]() | CopyMarkerPulseToRegister | Copy marker selected pulse to register D1/D2. | 24.00 |
![]() | CopyReferencePulses | Set reference pulses from measured pulse table. | 24.20 |
![]() | CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject) | — |
![]() | ExportPulseDescriptorWordFile | Create a PDW file from pulse analysis results. | 24.00 |
![]() | ExportPulseDescriptorWordFileFromRecording | Create a PDW file on pulse analysis results from entire recording | 24.00 |
![]() ![]() | ExtensionType | Returns the type for instances this measurement extension. Some tools are unable to use the generic methods provided on Agilent.SA.Vsa.Measurement class so this is provided as an alternative. | — |
![]() | ForceRebuildKeyMap | This method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | GetDeinterleaveMaxAmplitudes | Gets the maximum top level values for each emitter (dBm). | 23.00 |
![]() | GetDeinterleaveMaxFrequencies | Gets the maximum frequency values for each emitter (Hz). | 23.00 |
![]() | GetDeinterleaveMinAmplitudes | Gets the minimum top level values for each emitter (dBm). | 23.00 |
![]() | GetDeinterleaveMinFrequencies | Gets the minimum frequency values for each emitter (Hz). | 23.00 |
![]() | GetDeinterleaveModulationTypes | Gets the modulation type for each emitter. | 23.00 |
![]() | GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject) | — |
![]() | GetScoringReference | Gets the reference pulse profile. | 24.20 |
![]() | InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | Preset | Preset the Pulse measurement. | 19.00 |
![]() | RecallScoringReferenceFile | Read a scoring reference file. | 24.20 |
![]() | SavePulseDescriptorWordFile | Create a PDW file from pulse analysis results. | 20.00 |
![]() | SaveScoringReferenceFile | Create a scoring reference file. | 24.20 |
![]() | SetAllModulationTypes | Set or clear all modulation types that are detected | 20.00 |
![]() | SetCorrelationReference | Sets the correlation reference vector. | 23.20 |
![]() | SetCorrelationReferenceFromRegister | Sets the correlation reference vector from a data register | 23.20 |
![]() | SetDeinterleaveMaxAmplitudes | Sets the maximum top level values for each emitter (dBm). | 23.00 |
![]() | SetDeinterleaveMaxFrequencies | Sets the maximum frequency values for each emitter (Hz). | 23.00 |
![]() | SetDeinterleaveMinAmplitudes | Sets the minimum top level values for each emitter (dBm). | 23.00 |
![]() | SetDeinterleaveMinFrequencies | Sets the minimum frequency values for each emitter (Hz). | 23.00 |
![]() | SetDeinterleaveModulationTypes | Sets the modulation type values for each emitter. | 23.00 |
![]() | SetScoringReference | Sets the reference pulse profile. | 24.20 |
‡ This is the minimum 89600 VSA software version level needed to use this member. |