Cumulative Pulse Table (Advanced-Radar/Hopping)
Menu Path:
This trace is only available when the Synchronization Domain is Amplitude or the Pulsed checkbox is checked. If both of these are not true, the trace won't be available for selection.
The Cumulative Pulse Table is a type of Matrix Table that displays an accumulated list of pulse-specific result metrics for detected pulses since the last Measurement Restart.
When Statistics Enable is selected, the Cumulative Pulse Table lists and sequentially numbers each detected pulse in the current measurement. In continuous and single sweep mode, the table displays results for each detected pulse in the repeated measurement for the selected Display Length window. When the number of pulses in the table exceeds the Display Length, the table displays a window of pulses of Display Length, ending with the last detected pulse.
Sorting by metric
You can sort the table by any metric by left-clicking the metric name. Click again to toggle between ascending or descending order. Cancel sorting by right-clicking and selecting "Clear Sort".
See Also