Defines the segment sweep settings.
Enable segment sweep with SENS:SWE:TYPE SEGMent.
|
SENSe:Segment | ADD | BWIDth | CONTrol | COUNt | DELete | ALL | FREQuency | CENTer | SPAN | STARt | STOP | LIST | POWer | [LEVel] | CONTrol | [STATe] | SWEep | POINts | TIME | CONTrol | X | SPACing
|
Click on a keyword to view the command details.
Example: Upload and Download a Segment List
|
(Write-only) Adds a segment. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Segment number to add. If unspecified, value is set to 1. Segment numbers must be sequential. If a new number is added where one currently exists, the existing segment and those following are incremented by one. |
|
Examples |
Two Segments exist (1 and 2). The following command will add a new segment (1). The existing (1 and 2) will become (2 and 3) respectively. SENS:SEGM1:ADD |
|
Query Syntax |
Not applicable. Use Sense:Segment:Count to determine the number of segments in a trace. |
|
Not Applicable |
|
|
(Read-Write) Enables you to setup a segment sweep with arbitrary frequencies. The start and stop frequencies of each segment can overlap other segments. Also, each segment can have a start frequency that is greater than its stop frequency which causes a reverse sweep over that segment. Learn more about Arbitrary Segment Sweep. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
|
<ON | OFF> |
ON (or 1) - Allows the setup of arbitrary segment sweep. |
|
Examples |
SENS:SEGM:ARB ON |
|
Query Syntax |
SENSe<cnum>:SEGMent:ARBitrary? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
|
(Read-Write) Sets the IF Bandwidth for the specified segment. First set SENS:SEGM:BWIDth:CONTrol ON. All subsequent segments that are added assume the new IF Bandwidth value. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Segment number to modify. Choose any existing segment number. |
|
<num> |
IF Bandwidth in Hz. The list of valid IF Bandwidths is different depending on the PNA model. (Click to see the lists.) If an invalid number is specified, the analyzer will round up to the closest valid number. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SEGM:BWID 1KHZ sense2:segment2:bwidth:resolution max |
|
Query Syntax |
SENSe<cnum>:SEGMent<snum>:BWIDth[:RESolution]? |
|
Return Type |
Numeric |
|
Varies with PNA model. |
|
|
(Read-Write) Specifies whether the IF Bandwidth resolution can be set independently for each segment. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<ON | OFF> |
ON (or 1) - turns Bandwidth control ON. Bandwidth can be independently set for each segment. OFF (or 0) - turns Bandwidth control OFF. Use the channel IF bandwidth setting SENS:BWID. |
|
Examples |
SENS:SEGM:BWID:CONT ON sense2:segment:bwidth:control off |
|
Query Syntax |
SENSe<cnum>:SEGMent:BWIDth[:RESolution]:CONTrol? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
|
(Read-only) Queries the number of segments that exist in the specified channel. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
Examples |
SENS:SEGM:COUNt? |
|
Return Type |
Numeric |
|
1 segment |
|
|
(Write-only) Deletes the specified sweep segment. When ALL segments are deleted, SENS:SWE:TYPE is automatically set to Linear because there are no segments to sweep. |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Number of the segment to delete. If unspecified, value is set to 1 |
|
Examples |
SENS:SEGM:DEL |
|
Query Syntax |
Not applicable |
|
Not Applicable |
|
|
(Write-only) Deletes all sweep segments. When this command is executed, SENS:SWE:TYPE is automatically set to Linear because there are no segments to sweep. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
Examples |
SENS:SEGM:DEL:ALL |
|
Query Syntax |
Not applicable |
|
Not Applicable |
|
|
(Read-Write) Sets the Center Frequency for the specified segment. The Frequency Span of the segment remains the same. The Start and Stop Frequencies change accordingly. Note: All previous segment's Start and Stop Frequencies that are larger than the new Start Frequency are changed to the new Start Frequency. All following segment's start and stop frequencies that are smaller than the new Stop Frequency are changed to the new Stop Frequency. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Segment number to modify. Choose any existing segment number. |
|
<num> |
Center Frequency in Hz. Choose any number between the minimum and maximum frequency of the analyzer. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SEGM:FREQ:CENT 1MHZ |
|
Query Syntax |
SENSe<cnum>:SEGMent<snum>:FREQuency:CENTer? |
|
Return Type |
Numeric |
|
Stop Frequency of the previous segment. If first segment, start frequency of the analyzer. |
|
|
(Read-Write) Sets the Frequency Span for the specified segment. The center frequency of the segment remains the same. The start and stop frequencies change accordingly. Note: All previous segment's Start and Stop Frequencies that are larger than the new Start Frequency are changed to the new Start Frequency. All following segment's start and stop frequencies that are smaller than the new Stop Frequency are changed to the new Stop Frequency. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Segment number to modify. Choose any existing segment number. |
|
<num> |
Frequency Span in Hz. Choose any number between the minimum and maximum frequency of the analyzer. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SEGM:FREQ:SPAN 1MHZ |
|
Query Syntax |
SENSe<cnum>:SEGMent<snum>:FREQuency:SPAN? |
|
Return Type |
Numeric |
|
If first segment, frequency span of the analyzer. Otherwise 0. |
|
|
(Read-Write) Sets the Start Frequency for the specified sweep segment. Notes All other segment Start and Stop Frequency values that are larger than this frequency are changed to this frequency. To return the start and stop frequency of the entire sweep (all segments), Use SENS:FREQ:STARt? and SENS:FREQ:STOP? |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Segment number to modify. Choose any existing segment number. |
|
<num> |
Start Frequency in Hz. Choose any number between the minimum and maximum frequency of the analyzer. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SEGM:FREQ:STAR 1MHZ |
|
Query Syntax |
SENSe<cnum>:SEGMent<snum>:FREQuency:STARt? |
|
Return Type |
Numeric |
|
Stop Frequency of the previous segment. If first segment, start frequency of the analyzer. |
|
|
(Read-Write) Sets the Stop Frequency for the specified sweep segment. Notes All other segment Start and Stop Frequency values that are larger than this frequency are changed to this frequency. To return the start and stop frequency of the entire sweep (all segments), Use SENS:FREQ:STARt? and SENS:FREQ:STOP? |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Segment number to modify. Choose any existing segment number. |
|
<num> |
Stop Frequency in Hz. Choose any number between the minimum and maximum frequency of the analyzer. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SEGM:FREQ:STOP 1MHZ |
|
Query Syntax |
SENSe<cnum>:SEGMent<snum>:FREQuency:STOP? |
|
Return Type |
Numeric |
|
If first segment, stop frequency of the analyzer. Otherwise, start frequency of the segment. |
|
|
(Read-Write) Reads or writes the entire list of values in the segment sweep table. Note: For binary data transfer, specify 64-bit instead of 32-bit using FORMat[:DATA]. This is because higher frequencies used on PNA exceed the maximum value that can be represented by a 32-bit floating point number. When sending/receiving this data as binary (FORMat[:DATA] REAL,64), use FORMat:BORDer to specify the correct 'endianness' (byte ordering) corresponding to your programming environment / computer platform. |
||||||||||||||||
|
Parameters |
|
|||||||||||||||
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|||||||||||||||
|
<char> |
Choose from: SSTOP - Frequency values are Start and Stop for each segment. CSPAN - Frequency values are Center and Span for each segment. |
|||||||||||||||
|
<numSegs> |
Total number of sweep segments being input. This allows the PNA to determine how many values per-each-segment are in the input <data> block. |
|||||||||||||||
|
<data> |
A list of segments specified using either a comma-separated string of data, or an array of double (real,64) depending on the state of FORM:DATA. Each segment is specified with a minimum of 4 and maximum of 7 values consecutively. The set of values that specify each segment should be in the following order:
The first four data elements must always be supplied. After those values, data must be supplied for successive optional elements. For example, to set dwell time values, you must also supply IFBW values, because IFBW (#5) precedes dwell time (#6) in the array order. The IF Bandwidth, Sweep Time and Source Power Control settings do NOT affect the order in which elements are interpreted. The number of elements to supply for Power depends on the following two settings:
|
|||||||||||||||
|
Examples |
SENS:SEGM:LIST SSTOP,1,1,201,10E6,26.5E9,1E3,0,-10 1 segment, state ON, 201 points, 10 MHz to 26.5 GHz, 1kHz IFBW, 0 dwell time, -10 dBm (port powers coupled) sense2:segment:list? cspan See Upload and Download a Segment List example program |
|||||||||||||||
|
Query Syntax |
SENSe<cnum>:SEGMent:LIST? [char]. If unspecified, char is set to SSTOP. The number of data elements per segment returned will be 6 + total number of source ports, regardless of the IF Bandwidth, Sweep Time and Source Power Control settings. For the N5264A, which has no source ports, the query will return just 6 values per segment. For all other PNA models, the last elements in each segment correspond to the power level for each port. |
|||||||||||||||
|
Return Type |
Returns block data in the format specified by FORMat[:DATA]. |
|||||||||||||||
|
Not Applicable |
||||||||||||||||
|
(Read-Write) Sets the Port Power level for the specified sweep segment. First set SENS:SEGM:POW:CONTrol ON. When port power is Coupled, setting port power for one port will apply port power for all source ports. All subsequent segments that are added assume the new Power Level value. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Segment number to modify. Choose any existing segment number. |
|
<port> |
Port number of the source. If unspecified, value is set to 1. |
|
<num> |
Power level. Note: The range of settable power values depends on the PNA model and if source attenuators are installed. To determine the range of values, send SOUR:POW? MAX and SOUR:POW? MIN. (SOUR:POW:ATT:AUTO must be set to ON). Actual achievable leveled power depends on frequency. |
|
Examples |
SENS:SEGM:POW 0 |
|
Query Syntax |
SENSe<cnum>:SEGMent<snum>:POWer[<port>][:LEVel]? |
|
Return Type |
Numeric |
|
0 |
|
|
(Read-Write) Specifies whether Power Level can be set independently for each segment. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<ON | OFF> |
ON (or 1) - turns Power Level control ON. Power level can be set for each segment. |
|
Examples |
SENS:SEGM:POW:CONT ON |
|
Query Syntax |
SENSe<cnum>:SEGMent:POWer[:LEVel]:CONTrol? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
|
(Read-Write) Turns the specified sweep segment ON or OFF. At least ONE segment must be ON or Sweep Mode is automatically set to Linear. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Segment number to be turned ON or OFF |
|
<ON | OFF> |
ON (or 1) - turns segment ON. |
|
Examples |
SENS:SEGM ON |
|
Query Syntax |
SENSe<cnum>:SEGMent<snum>[:STATe]? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
|
(Read-Write) Sets the number of data points for the specified sweep segment. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Any existing segment number. If unspecified, value is set to 1 |
|
<num> |
Number of points in the segment. The total number of points in all segments cannot exceed 20001. A segment can have as few as 1 point. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SEGM:SWE:POIN 51 |
|
Query Syntax |
SENSe<cnum>:SEGMent<snum>:SWEep:POINts? |
|
Return Type |
Numeric |
|
21 |
|
|
(Read-Write) Sets the time the analyzer takes to sweep the specified sweep segment. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<snum> |
Any existing segment number. |
|
<num> |
Sweep time in seconds. Choose a number between 0 and 100 Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SEGM:SWE:TIME 1ms |
|
Query Syntax |
SENSe<cnum>:SEGMent<snum>:SWEep:TIME? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
(Read-Write) Specifies whether Sweep Time can be set independently for each sweep segment. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<ON | OFF> |
ON (or 1) - turns Sweep Time control ON. Sweep Time can be set for each segment. |
|
Examples |
SENS:SEGM:SWE:TIME:CONT ON |
|
Query Syntax |
SENSe<cnum>:SEGMent:SWEep:TIME:CONTrol? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
|
(Read-Write) Sets X-axis spacing ON or OFF |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
LINear - turns X-axis point spacing OFF OBASe - turns X-axis point spacing ON |
|
Examples |
SENS:SEGM:X:SPACing LIN |
|
Query Syntax |
SENSe<cnum>:SEGMent:X:SPACing? |
|
Return Type |
Character |
|
LINear |
|
Last Modified:
|
20-Aug-2013 |
Fixed error in finder map. |
|
7-May-2012 |
Removed preset |
|
30-Aug-2011 |
Removed Snum from X:Spacing |
|
27-Oct-2009 |
Added Segment:List note |
|
29-Apr-2009 |
Added List command (8.6) |
|
13-May-2008 |
Fixed segment delete links |
|
21-Jun-2007 |
Increased max number of points |