Sets and reads the PNA Preferences settings.
| 
 SYSTem:PREFerences | DEFault | ITEM | KEYS | MCMethod | MCPreset | MRU | OFFSet | RCV | SRC | PSRTrace | QSTart | RECeivers | CERRor | RTOF 
  | 
Click on a keyword to view the command details.
See Also
| 
 (Write-only) Resets the PNA preferences to their default settings. Some default settings vary depending on the PNA Model. Learn more about PNA Preferences.  | 
|
| 
 Examples  | 
 SYST:PREF:DEF  | 
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|
| 
 (Read-Write) Set and return whether External Devices remain activated or are de-activated when the PNA is Preset or when a Instrument State is recalled. This setting remains until changed again using this command, or until the hard drive is changed or reformatted.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: OFF (0) External devices remain active when the PNA is Preset or when a Instrument State is recalled. ON (1) External devices are de-activated (SYST:CONF:EDEV:STAT to OFF) when the PNA is Preset or when a Instrument State is recalled.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:EDEV:DPOL 1  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:EDEV:DPOLicy?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 ON or 1  | 
|
| 
 (Read-Write) Sets whether a Swept IMD or IMDx calibration can exceed the stop frequency limit of an ECal module. Learn more.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) Allow extrapolation. OFF (0) Do NOT allow extrapolation.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:EEXT 1 system:preferences:item:eextrapolate OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:EEXTrapolate?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF  | 
|
| 
 (Read-Write) Sets the default group delay aperture setting. Learn more about group delay aperture.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) Sets default group delay aperture to 2 points. OFF (0) Sets default group delay aperture to 11 points.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:GDELay:TWOPoint 1  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:GDELay:TWOPoint?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF  | 
|
| 
 (Read-Write) Set and return whether the keys are displayed or not.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) – Turn keys on. OFF (0) – Turn keys off.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:KEYS 1 system:preferences:item:keys OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:KEYS?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF (0)  | 
|
| 
 (Read-Write) Set and return whether the Coupled Markers setting controls the ON|OFF state of markers that are coupled. Learn more about Coupled Markers. Refer also to CALC:MARK:COUP:STATe ON.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) – With Coupled Markers ON, when a marker is turned on, the same-numbered marker on all coupled traces will also be turned on. Likewise, turning off a marker will turn it off on all coupled traces. OFF (0) – Turning a marker on or off will have no effect on the markers on other traces.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:MCC 1 system:preferences:item:mccontrol OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:MCControl?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF (0)  | 
|
| 
 (Read-Write) Set and return whether Coupled Markers is set to Channel or All after Preset. Learn more about Coupled Markers. Refer also to CALC:MARK:COUP:STATe ON and SYST:PREF:ITEM:MCPR ON.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) – Marker Coupling Method is set to Channel after Preset. OFF (0) – Marker Coupling Method is set to ALL after Preset.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:MCM 1 system:preferences:item:mcmethod OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:MCMethod?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF (0)  | 
|
| 
 (Read-Write) Set and return whether Coupled Markers is set to ON or OFF after Preset. Learn more about Coupled Markers.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: OFF (0) – Coupled Markers is OFF after Preset. ON (1) – Coupled Markers is ON after Preset.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:MCPR 1 system:preferences:item:mcpreset OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:MCPReset?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF (0)  | 
|
| 
 (Read-Write) Sets and reads the state of the memory data interpolation default preference. The PNA will return to the default interpolation state after a Preset, creating a new trace, or closing the PNA application. Learn more.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: 0 - OFF - Set memory interpolation to OFF as the default. 1 - ON - Set memory interpolation to ON as the default.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:MINT 1  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:MINTerpolate?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 0  | 
|
| 
 (Read-Write) Set and return whether to list files for recall on softkeys by most-recently used or alphabetically.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) – Recall softkeys show most recently-used files. OFF (0) – Recall softkeys show alphabetically-ordered files.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:MRU 1 system:preferences:item:mru OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:MRU?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF (0)  | 
|
| 
 (Read-Write) Set and return whether to offset the test port receivers by the amount of receiver attenuation. Learn more. To send this command using the PNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the PNA took the command. This setting remains until changed again using this command, or until the hard drive is changed or reformatted.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) Offset the test port receivers OFF (0) Do NOT offset the test port receivers  | 
| 
 Examples  | 
 SYST:PREF:ITEM:OFFS:RCV 1  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:OFFSet:RCV?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 PNA-L and E836xB: OFF (does NOT offset the display). PNA-X: ON (offsets the display).  | 
|
| 
 (Read-Write) Set and return whether to offset the reference receiver by the amount of source attenuation. Learn more. To send this command using the PNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the PNA took the command. This setting remains until changed again using this command, or until the hard drive is changed or reformatted.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) Offset the reference receivers. OFF (0) Do NOT Offset the reference receivers.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:OFFS:SRC 1  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:OFFSet:SRC?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 All models: ON (offset the display).  | 
|
| 
 (Read-Write) Set and return the Preset Power ON/OFF state. Learn more. This setting remains until changed again using this command, or until the hard drive is changed or reformatted.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <char>  | 
 Choose from: ON - Instrument Preset always turns RF power ON. AUTO - When the current power setting is OFF, leave power OFF after Preset. When the current power setting is ON, turn power ON after Preset.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:PRE:POW ON  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:PREset:POWer[:STATe]?  | 
| 
 Return Type  | 
 Character  | 
| 
 ON  | 
|
| 
 (Read-Write) At the end of a power sweep, while waiting to trigger the next sweep, maintain source power at either the start power level or at the stop power level. To send this command using the PNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the PNA took the command. This setting remains until changed again using this command, or until the hard drive is changed or reformatted.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <char>  | 
 Choose from: STARt - Maintain source power at the start power level. STOP - Maintain source power at the stop power level.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:PSRT STOP  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:PSRTrace?  | 
| 
 Return Type  | 
 Character  | 
| 
 STARt  | 
|
| 
 (Read-Write) This command controls the on/off state of the preference, "On PRESET show Quick Start dialog".  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) Display the Quick Start dialog on PRESET. OFF (0) Do not display the Quick Start dialog on PRESET.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:QST 1  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:QST?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF  | 
|
| 
 (Read-Write) Set and return whether to display receiver overload warnings. Learn more.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) Display overload warnings, OFF (0) Do NOT display overload warnings.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:REC:CERR 1 system:preferences:item:receivers:cerror:state OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:RECeivers:CERRor[:STATe]?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 ON  | 
|
| 
 (Read-Write) Set and return whether to turn source power OFF when a receiver is overloaded. Learn more.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) Turn OFF source power to ALL ports when a receiver is overloaded. OFF (0) Power remains ON when a receiver is overloaded.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:REC:OVER:POW 1 system:preferences:item:receivers:overload:power:state OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:RECeivers:OVERload:POWer[:STATe]?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF (0)  | 
|
| 
 (Read-Write) Set and return whether to draw limits lines in Red or the trace color.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) All Limit lines are drawn in Red. OFF (0) Limit lines are drawn the same color as the trace.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:REDL 1 system:preferences:item:redlimits OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:REDLimits?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF  | 
|
| 
 (Read-Write) Set and return whether to treat marker 10 as a reference marker. Learn more.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) Marker 10 is always a reference marker (Pre A.10.40 behavior). OFF (0) Marker 10 is just another marker. See Reference Marker commands  | 
| 
 Examples  | 
 SYST:PREF:ITEM:REFM 1 system:preferences:item:refmarker OFF  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:REFMarker?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF  | 
|
| 
 (Read-Write) For single-band frequency or segment sweeps ONLY, specify whether to turn RF power ON or OFF during a retrace. Learn more about RF power during sweep retrace. To send this command using the PNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the PNA took the command. This setting remains until changed using this command, or until the hard drive is changed or reformatted.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <char>  | 
 Choose from: AUTO: Power is left ON during retrace of single-band frequency or segment sweeps ONLY. OFF: Power is turned OFF during retrace of single-band frequency or segment sweeps ONLY.  | 
| 
 Examples  | 
 SYST:PREF:ITEM:RETR:POW OFF system:preferences:item:retrace:power auto  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:RETRace:POWer?  | 
| 
 Return Type  | 
 Character  | 
| 
 AUTO  | 
|
| 
 (Read-Write) Set and return whether to display limit line failures as red trace segments or red data points (dots). Learn more.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bool>  | 
 Choose from: ON (1) Display failures as red trace segments. (Red Trace On Fail). OFF (0) Display failures as red data points (dots).  | 
| 
 Examples  | 
 SYST:PREF:ITEM:RTOF 1  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:RTOF?  | 
| 
 Return Type  | 
 Boolean  | 
| 
 OFF  | 
|
| 
 (Read-Write) Sets the default setting for the Noise Tuner switch. This is the setting that occurs when a new channel is created. Learn more. This command will return an error on PNA models with a built-in Noise tuner. To send this command using the PNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the PNA took the command. This setting remains until changed using this command, or until the hard drive is changed or reformatted.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <string>  | 
 Name of the switch to set. Choose from: 
  | 
| 
 <int>  | 
 Value to set. Choose from: 0 Sets the default (preset) to INTERNAL 1 Sets the default (preset) to EXTERNAL  | 
| 
 Examples  | 
 SYST:PREF:ITEM:SWIT:DEF "Port1NoiseTuner" 1 'Write system:preferences:item:switch:def? "Port1NoiseTuner" 'Read  | 
| 
 Query Syntax  | 
 SYSTem:PREFerences:ITEM:SWITch:DEF? <switch>  | 
| 
 Return Type  | 
 Integer  | 
| 
 1 (External)  | 
|