:DIFF:THReshold:GENeral:BASE
Command Syntax
:DIFFN:THReshold:GENeral:BASE <amplitude>
<amplitude> is a double.
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:THReshold:GENeral:BASE?
Description
For the indicated differential waveform, sets or queries the General threshold's custom base-level setting. The top and base levels are used to locate a waveform's lower, middle, and upper threshold levels for measurements. Specify the level in volts. Use :DIFF:THReshold:GENeral:TOP to set or query a custom top level.
Before this user-defined base level can be applied to measurements, use the :DIFF:TBASe:GENeral:METHod command to select user-defined top-base definitions.
Example Command Sequence
:DIFF3_1:THReshold:GENeral:TRACking OFF :DIFF3_1:TBASe:GENeral:METHod ABSolute :DIFF3_1:THReshold:GENeral:BASE -125E-3 :DIFF3_1:THReshold:GENeral:TOP 125E-3