:DIFF:THReshold:RFALl:TRACking

Command Syntax

:DIFFN:THReshold:RFALl:TRACking  {{ON | 1} | {OFF | 0}}

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:THReshold:RFALl:TRACking?

Query Response

{1 | 0}

Description

Specifies whether a signal tracks the Rise/Fall threshold's global threshold definition or uses its own threshold definition.

The global threshold definition is set using the :MEASure:THReshold:RFALl commands (see Threshold Configuration Commands).

Example Command Sequence

:DIFF2:THReshold:RFALl:TRACking OFF
:DIFF2:THReshold:RFALl:METHod ABSolute
:DIFF2:THReshold:RFALl:UPPer 125E-3
:DIFF2:THReshold:RFALl:LOWer -125E-3