:DIFF:THReshold:GENeral:STZero

Command Syntax

:DIFFN:THReshold:GENeral:STZero  {{ON | 1} | {OFF | 0}}

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:THReshold:GENeral:STZero?

Query Response

{1 | 0}

Description

When you select the ± Hysteresis threshold definition for the selected signal (see :DIFF:THReshold:GENeral:METHod), you can turn ON the :DIFF:THReshold:GENeral:STZero setting to move thresholds within ±10 mV to zero. This feature is useful for differential signals.