:DIFF:THReshold:RFALl:PAM:PAMLevel:LEVel
Command Syntax
:DIFFN:THReshold:RFALl:PAM:PAMLevel:LEVel{0:3} <amplitude>
Where <amplitude> is a double.
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:THReshold:RFALl:PAM:PAMLevel:LEVel{0:3}?
Description
When specifying PAM rise/fall levels and you have selected the Absolute level method for the selected signal (see :DIFF:TBASe:RFALl:METHod), this command sets or queries the PAM level values.
Use the :DIFF:THReshold:RFALl:PAM:ASLevels command to automatically set the PAM levels.