:DIFF:THReshold:RFALl:PLOWer

Command Syntax

:DIFFN:THReshold:RFALl:PLOWer  <percent>

<percent> is a decimal number from -25.0 to +125.0.

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:THReshold:RFALl:PLOWer?

Description

When the threshold method is a custom PERCent between top and base (see :DIFF:THReshold:RFALl:METHod), the :DIFF:THReshold:RFALl:PLOWer command sets or queries the custom lower percent value.

Example Command Sequence

:DIFF2:THReshold:RFALl:TRACking OFF
:DIFF2:THReshold:RFALl:METHod PERCent
:DIFF2:THReshold:RFALl:PUPPer 125E-3
:DIFF2:THReshold:RFALl:PLOWer -125E-3