:DIFF:THReshold:GENeral:TRACking
Command Syntax
:DIFFN:THReshold:GENeral:TRACking {{ON | 1} | {OFF | 0}}
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:THReshold:GENeral:TRACking?
Query Response
{1 | 0}
Description
Specifies whether a signal tracks the General threshold's global threshold definition or uses its own threshold definition.
The global threshold definition is set using the :MEASure:THReshold:GENeral commands (see Threshold Configuration Commands).
Example Command Sequence
:DIFF2:THReshold:GENeral:TRACking OFF :DIFF2:THReshold:GENeral:METHod ABSolute :DIFF2:THReshold:GENeral:UPPer 125E-3 :DIFF2:THReshold:GENeral:MIDDle 0E0 :DIFF2:THReshold:GENeral:LOWer -125E-3