:DIFF:THReshold:GENeral:HYSTeresis
Command Syntax
:DIFFN:THReshold:GENeral:HYSTeresis <plus_or_minus_value>
<plus_or_minus_value> is a double.
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:THReshold:GENeral:HYSTeresis?
Description
When the :DIFF:THReshold:GENeral:METHod setting is HYSTeresis, this command sets the user-defined ±hysteresis value for the waveform source.
Use the :DIFF:THReshold:GENeral:MIDDle command to enter the center threshold level.
Example Command Sequence
:DIFF3_1:THReshold:GENeral:TRACking OFF :DIFF3_1:THReshold:GENeral:METHod HYSTeresis :DIFF3_1:THReshold:GENeral:HYSTeresis 125E-3 :DIFF3_1:THReshold:GENeral:MIDDle 0E0