:DISK:SETup:RECall
Command Syntax
:DISK:SETup:RECall "filename"
Description
Loads a setup file into Infiniium 2026. Use the :DISK:SETup:SAVE command to save a state setup file. Setup files use the .seti file extension and by default are saved in the %USER_DATA_DIR%\Setups folder.
C:\Users\user\Documents\Keysight\Infiniium\Setups
Before recalling a setup file, you may want to change these include settings:
:DISK:SETup:RECall:GENeral(general settings, default isON):DISK:SETup:RECall:TRIGger(trigger settings, default isON):DISK:SETup:RECall:PROBes(probe settings, default isOFF):DISK:SETup:RECall:CSKew(channel skew settings, default isOFF):DISK:SETup:RECall:PREFerences(preference settings, default isOFF):DISK:SETup:RECall:ICONnection(instrument connection settings, default isOFF)
To assign the loading of a setup file to the Multi-Purpose button, use the :SYSTem:MPButton:FUNCtion command.