:DISK:SETup:RECall:ICONnection
Command Syntax
:DISK:SETup:RECall:ICONnection {ON | OFF}
Query Syntax
:DISK:SETup:RECall:ICONnection?
Description
Enables or disables the loading of instrument configuration settings when a setup file is recalled using the :DISK:SETup:RECall command.
Most often, you will be connected to a different oscilloscope. However, if you are using Infiniium offline on different computers, you may want to include these settings when you connect to the same oscilloscope.
OFF is the default setting for this option.
Instrument configuration settings are always saved with an instrument state file.