:DISK:SETup:RECall:PROBes
Command Syntax
:DISK:SETup:RECall:PROBes {ON | OFF}
Query Syntax
:DISK:SETup:RECall:PROBes?
Description
Enables or disables the loading of probe settings when a setup file is recalled using the :DISK:SETup:RECall command.
Probe settings are tied to individual probes which are not likely to be the same on different oscilloscopes. Even when the same probe models are used on the same input channels, calibrations can make the settings different.
OFF is the default setting for this option.
Probe settings are always saved with a setup file.