:DISK:SETup:RECall:PREFerences
Command Syntax
:DISK:SETup:RECall:PREFerences {ON | OFF}
Query Syntax
:DISK:SETup:RECall:PREFerences?
Description
Enables or disables the loading of preference settings when a setup file is recalled using the :DISK:SETup:RECall command.
Preferences are user settings that are not changed by a Default Setup (see *RST (Reset) or :SYSTem:DEFault) but are changed by a Factory Default (see :SYSTem:FACTory).
OFF is the default setting for this option.
Preference settings are always saved with a setup file.