:DISK:SETup:SAVE

Command Syntax

:DISK:SETup:SAVE "filename.seti"

Description

Saves an Infiniium setup file with the given filename (*.seti). Setup files can be reloaded into Infiniium using the :DISK:SETup:RECall command.

When the setup file is re-loaded into the application, the file restores all InfiniiumInfiniium 2026's settings to those in place at the time that the file was saved. One example of using a setup file is to quickly scale the JTF graph's x and y axis.

When you save a setup file, all the Infiniium's settings are saved to the file you have selected, including:

  • Type of measurements currently running
  • Markers (if used)
  • Horizontal and vertical settings
  • Trigger configuration
  • Display setup
  • Functions
  • Fixture Deskew data
  • Instrument connection

By default, the files are saved in the user data \Setups folder.

C:\Users\user\Documents\Keysight\Infiniium\Setups

Setup files must have the extension .seti. If you do not specify an extension or use a different extension, Infiniium may not recognize the file as a setup file and you may have trouble saving or finding the setup file.

Be sure to save an Infiniium setup file when saving jitter data or color grade-gray scale memory files. This is because horizontal scale and delay information are not saved in jitter data or color grade-gray scale memory files. If you plan on loading these memory files back into the Infiniium, you will also need to load the associated Infiniium setup file.

Infiniium maintains its current settings in a system file, which is not the same as a setup file. To ensure that the settings are correctly saved, close the Infiniium application from the File menu using the Exit command.