:DISK:SETup:RECall:GENeral
Command Syntax
:DISK:SETup:RECall:GENeral {ON | OFF}
Query Syntax
:DISK:SETup:RECall:GENeral?
Description
Enables or disables the loading of general settings when a setup file is recalled using the :DISK:SETup:RECall command.
General settings include displayed channels, vertical scales, horizontal scales, acquisitions, content window layouts, and more.
ON is the default setting for this option.
General settings are always saved with a setup file.