:DISK:SETup:RECall:CSKew
Command Syntax
:DISK:SETup:RECall:CSKew {ON | OFF}
Query Syntax
:DISK:SETup:RECall:CSKew?
Description
Enables or disables the loading of channel skew settings when a setup file is recalled using the :DISK:SETup:RECall command.
Channel skew settings are tied to individual input channel hardware and are not likely to be valid for different oscilloscopes.
OFF is the default setting for this option.
Channel skew settings are always saved with a setup file.