:DISK:SETup:RECall:TRIGger
Command Syntax
:DISK:SETup:RECall:TRIGger {ON | OFF}
Query Syntax
:DISK:SETup:RECall:TRIGger?
Description
Enables or disables the loading of trigger settings when a setup file is recalled using the :DISK:SETup:RECall command.
Trigger settings are important for capturing similar waveforms on different devices under test (DUTs) and on different oscilloscopes. It may be that you are interested only in restoring the trigger settings from a setup file.
ON is the default setting for this option.
Trigger settings are always saved with a setup file.