:FUNCtion:PARameters:FFEQualizer:BANDwidth

Command Syntax

:FUNCtionN:PARameters:FFEQualizer:BANDwidth <bandwidth>

<bandwidth> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:FFEQualizer:BANDwidth?

Description

Specifies the bandwidth, in Hertz, of a Linear Equalizer operator (LFE) (:FUNCtion:FOPerator). The :FUNCtion:PARameters:FFEQualizer:BANDwidth:AUTO child command must be set OFF, before you can manually set the bandwidth.

Example Command Sequence

:FUNCtion2:FOPerator FFEQualizer
:FUNCtion2:PARameters:FFEQualizer:TAPS:AUTO ON
:FUNCtion2:PARameters:FFEQualizer:TAPS:COUNt 5
:FUNCtion2:PARameters:FFEQualizer:NPRecursors 3
:FUNCtion2:PARameters:FFEQualizer:BANDwidth:AUTO OFF
:FUNCtion2:PARameters:FFEQualizer:BANDwidth 8.0E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.

Child Commands