:FUNCtion:PARameters:FFEQualizer:TSPacing:TIME

Command Syntax

:FUNCtionN:PARameters:FFEQualizer:TSPacing:TIME <seconds>

<seconds> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Specifies tap spacing in seconds for a Linear Equalizer operator (LFE) (:FUNCtion:FOPerator). To select tap spacing in seconds or taps-per-bit, use the :FUNCtion:PARameters:FFEQualizer:TSPacing command. This command is not valid in automatic tap configuration mode (:FUNCtion:PARameters:FFEQualizer:TAPS:AUTO).

Example Command Sequence

:FUNCtion2:FOPerator FFEQualizer
:FUNCtion2:PARameters:FFEQualizer:TAPS:AUTO OFF
:FUNCtion3:PARameters:FFEQualizer:TAPS "-4.0733E-2, 1.04365, 3.851E-3, -3.782E-3, -7.04E-4"
:FUNCtion3:PARameters:FFEQualizer:TAPS:NORMalize
:FUNCtion2:PARameters:FFEQualizer:TSPacing SEConds
:FUNCtion2:PARameters:FFEQualizer:TSPacing:TIME 51.0E-12
:FUNCtion2:PARameters:FFEQualizer:BANDwidth:AUTO OFF
:FUNCtion2:PARameters:FFEQualizer:BANDwidth 8.0E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.

Parent Command