:FUNCtion:PARameters:FFEQualizer:DCGain?
Query Syntax
:FUNCtionN:PARameters:FFEQualizer:DCGain?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Returns the DC gain of a Linear Equalizer operator (LFE) (:FUNCtion:FOPerator).