:FUNCtion:PARameters:FFEQualizer:TAPS:RECalculate
Command Syntax
:FUNCtionN:PARameters:FFEQualizer:TAPS:RECalculate
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Initiates a re-calculation of the tap values for a Linear Equalizer operator (LFE) (:FUNCtion:FOPerator). Automatic tap configuration must be enabled (:FUNCtion:PARameters:FFEQualizer:TAPS:AUTO).