:FUNCtion:PARameters:FFEQualizer:BANDwidth:AUTO

Command Syntax

:FUNCtionN:PARameters:FFEQualizer:BANDwidth:AUTO {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:FFEQualizer:BANDwidth:AUTO?

Query Response

{1 | 0}

Description

Turns on or off automatic bandwidth setting for a Linear Equalizer operator (LFE) (:FUNCtion:FOPerator). When on, the bandwidth of the operator tracks the bandwidth of the source. When off, use the parent command (:FUNCtion:PARameters:FFEQualizer:BANDwidth) to enter the bandwidth.

Example Command Sequence

:FUNCtion2:FOPerator FFEQualizer
:FUNCtion2:PARameters:FFEQualizer:TAPS:AUTO ON
:FUNCtion2:PARameters:FFEQualizer:TAPS:COUNt 5
:FUNCtion2:PARameters:FFEQualizer:NPRecursors 3
:FUNCtion2:PARameters:FFEQualizer:BANDwidth:AUTO OFF
:FUNCtion2:PARameters:FFEQualizer:BANDwidth 8.0E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.

Parent Command