Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:FUNCtion:PARameters:FFEQualizer:PRESets:SELections?

Linear Equalizer Parameters Commands
  • :FUNCtion:PARameters:FFEQualizer:BANDwidth
  • :FUNCtion:PARameters:FFEQualizer:BANDwidth:AUTO
  • :FUNCtion:PARameters:FFEQualizer:BWMode
  • :FUNCtion:PARameters:FFEQualizer:CLKDelay
  • :FUNCtion:PARameters:FFEQualizer:DCGain?
  • :FUNCtion:PARameters:FFEQualizer:IMPulse
  • :FUNCtion:PARameters:FFEQualizer:NPRecursors
  • :FUNCtion:PARameters:FFEQualizer:PRESets
  • :FUNCtion:PARameters:FFEQualizer:PRESets:SELections?
  • :FUNCtion:PARameters:FFEQualizer:STEP
  • :FUNCtion:PARameters:FFEQualizer:TAPS
  • :FUNCtion:PARameters:FFEQualizer:TAPS:AUTO
  • :FUNCtion:PARameters:FFEQualizer:TAPS:COUNt
  • :FUNCtion:PARameters:FFEQualizer:TAPS:NORMalize
  • :FUNCtion:PARameters:FFEQualizer:TAPS:RECalculate
  • :FUNCtion:PARameters:FFEQualizer:TFUNction
  • :FUNCtion:PARameters:FFEQualizer:TSPacing
  • :FUNCtion:PARameters:FFEQualizer:TSPacing:TIME
  • :FUNCtion:PARameters:FFEQualizer:TSPacing:TPUI
  • :FUNCtion:PARameters:FFEQualizer:WIDTh

Query Syntax

:FUNCtion:PARameters:FFEQualizer:PRESets:SELections?

Query Response

"preset name, preset name, preset name, …"

Description

Returns a string which is a comma-separated list of all saved presets for the Linear Feedforward Equalizer operator (LFE). Use the :FUNCtion:PARameters:FFEQualizer:PRESets command to load one of these presets.

Parent Command

  • :FUNCtion:PARameters:FFEQualizer:PRESets