:FUNCtion:PARameters:FFEQualizer:PRESets
Command Syntax
:FUNCtion:PARameters:FFEQualizer:PRESets <string>
Description
Loads a previously saved a preset for a Linear Feedforward Equalizer operator (LFE). The preset configures the operator to your saved settings. To query which presets are available for loading, use the :FUNCtion:PARameters:FFEQualizer:PRESets:SELections? query.
Presets can only be saved from the operator's Setup dialog box. There is no programming command for this task.
Example Command
:FUNCtion:PARameters:FFEQualizer:PRESets "MyPreset" // Load a saved preset.