:MEASure:PJITter:DIMensions

Command Syntax

:MEASure:PJITterN:DIMensions  <left_col>,<right_col>

Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.

<left_col> and <right_col> are whole or decimal numbers.

Query Syntax

:MEASure:PJITterN:DIMensions?

Description

Specifies the proportions of the left-column measurement tables and the right-column measurement histograms within the PAM Jitter content window.

The width of a column is the number specified, divided by the sum of all the numbers specified, times the total display width. For example, to specify left and right column widths of 60% and 40%, respectively, you can use the dimensions of "0.6,0.4", "6,4", "60,40", etc.