:MEASure:PJITter:RJComp:VALue
Command Syntax
:MEASure:PJITterN:RJComp:VALue <compensation_RJ_value>
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
<compensation_RJ_value> is a double.
Query Syntax
:MEASure:PJITterN:RJComp:VALue?
Description
When using custom RJ compensation (see :MEASure:PJITter:RJComp:MODE), this command lets you specify the appropriate custom RJ value.