:MEASure:PJITter:RJComp:MODE

Command Syntax

:MEASure:PJITterN:RJComp:MODE {OFF | CUSTom | AUTomatic}

Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.

Query Syntax

:MEASure:PJITterN:RJComp:MODE?

Description

This command selects the RJ compensation option:

OFF
Disables RJ compensation.
CUSTom
Enables a user-defined value for RJ compensation.
If there are known contributors to random jitter, you can use RJ Compensation to compensate or remove jitter from the measurement results.
Use the :MEASure:PJITter:RJComp:VALue command to specify the appropriate RJ compensation value.
AUTomatic
Uses the RN compensation values specified by the :MEASure:PJITter:RJComp:RN:LEVel command.