:MEASure:PJITter:MPCount

Command Syntax

:MEASure:PJITterN:MPCount <report_count>
            

Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.

<report_count> is an integer from 200 to 1,000,000. The default is 10,000.

Query Syntax

:MEASure:PJITterN:MPCount?

Description

This command specifies the number of times the PAM Jitter measurements must be made before a result is reported

The IEEE 802.3bs standard (and other standards) can specify these measurements must be made 10,000 times.