:MEASure:PJITter:UNITs
Command Syntax
:MEASure:PJITterN:UNITs {SECond | UINTerval}
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
Query Syntax
:MEASure:PJITterN:UNITs?
Description
Sets the time units for PAM jitter measurements. The units can be seconds (SECond) or unit interval (UINTerval).