:MEASure:PJITter:FILE:NAME
Command Syntax
:MEASure:PJITterN:FILE:NAME <filename>
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
<filename> is the quoted data pattern file name.
Description
When FILE is selected to specify the data pattern (see :MEASure:PJITter:MODE), this command specifies the data pattern file name to load and use.
The format of this file is proprietary. For help developing custom files, contact Keysight Technical Support and ask for an Application Engineer.
To reload the data pattern file, use the :MEASure:PJITter:FILE:RELoad command.