:MEASure:PJITter:RJComp:RN:LEVel
Command Syntax
:MEASure:PJITterN:RJComp:RN:LEVel{0|1|2|3} <RN_compensation_value>
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
<RN_compensation_value> is a double.
Query Syntax
:MEASure:PJITterN:RJComp:RN:LEVel{0|1|2|3}?
Description
When using AUTomatic RJ compensation (see :MEASure:PJITter:RJComp:MODE), this command specifies the RN compensation value to use for each level.