:MHIStogram:ANNotations
Command Syntax
:MHIStogramN:ANNotations {ON | OFF | 1 | 0}
Where N identifies one of four possible measurement histograms {1:4}. For example, :MHIStogram3.
Query Syntax
:MHIStogramN:ANNotations?
Query Response
{1 | 0}
Description
Turns on or off the display of the Total Hits and Hits/Acq values on the histogram plot. When Measure All is selected for a measurement, there can be multiple hits per acquisition.