:MHIStogram:INCRement?
Query Syntax
:MHIStogramN:INCRement?
Where N identifies one of four possible measurement histograms {1:4}. For example, :MHIStogram3.
Description
Returns the width of each bin in the measurement histogram.
Use the :MHIStogram:POINts? query to return the number of bins in the measurement histogram.
To return the number of measurement results in each bin, use the :MHIStogram:ASCii:DATA? or :MHIStogram:INTeger:DATA? queries.