:MHIStogram:BINS

Command Syntax

:MHIStogramN:BINS  <number>

<number> is an integer from 101 to 8001.

Where N identifies one of four possible measurement histograms {1:4}. For example, :MHIStogram3.

Query Syntax

:MHIStogramN:BINS?

Description

You can control the resolution of histogram plot and statistics by changing the number of bins used in the histogram. A bin is the width of one of the histogram bars.

An odd number of bins is preferred so that floating-point values in the middle of the dynamic range ((top + bottom) / 2) do not land on a bin boundary. In the front panel graphical user interface, default, minimum, maximum, lower, and higher values are all set to an odd number of bins.