:MHIStogram:SCALe
Command Syntax
:MHIStogramN:SCALe {LINear | LOG}
Where N identifies one of four possible measurement histograms {1:4}. For example, :MHIStogram3.
Query Syntax
:MHIStogramN:SCALe?
Description
Sets the selected measurement histogram's vertical scale to linear or logarithmic. The default setting is LINear.