:MHIStogram:ORIGin?

Query Syntax

:MHIStogramN:ORIGin?

Where N identifies one of four possible measurement histograms {1:4}. For example, :MHIStogram3.

Description

Returns the center value of the first histogram bin (bucket). Knowing the origin value and width value of each histogram bin (:MHIStogram:INCRement?), you can determine the center values (and range) of each histogram bin.