:MHIStogram:SOURce:LOCation

Command Syntax

:MHIStogramN:SOURce:LOCation  <measurement_source>
            

Where N identifies one of four possible measurement histograms {1:4}. For example, :MHIStogram3.

Where <measurement_source> is the number of the measurement according to the top-to-bottom order in the Measurement results window.

Query Syntax

:MHIStogramN:SOURce:LOCation?

Description

Selects the measurement source by its number in the top-to-bottom order of the Measurement results window.